Other emissions to the atmosphere, discharges to water and releases to land
Prysmian has assessed and disclosed the most significant impacts at Group level. At local level, each operating site identifies and measures its environmental aspects and impacts, and monitoring is periodically conducted in accordance with applicable legal requirements and specific licenses and verified both internally and externally through HSE audits.
With regard to air emissions, great attention is paid to greenhouse gas (GHG) emissions primarily linked to the use of energy sources and, to a very limited extent, to the use of greenhouse gases in certain production phases. These include the impact from the combustion processes, whose emissions are disclosed in terms of CO2eq emissions.
Further information is available in the GHG Statement 2022.