A closer look at the EU Gigabit Infrastructure Act
Recently, the European Commission published its Gigabit Infrastructure Act (GIA) proposal. The intention: to contribute to deployment of networks that can meet users’ current and future demands. The EC proposes to support this by facilitating access to network operators’ and public institutions’ physical infrastructure, improving civil works coordination, and uniform, digitally accessible permit procedures.
In 2022 the European Parliament stated that the EU's digital infrastructure is in need of “substantial updating, with just 25 % of people in the EU being able to connect to a 5G network, compared to 76 % (…) in the United States”. The parliament also observed that the EU lacks “high-performance digital infrastructure with interoperable data spaces, high transmission rates and volumes, reliability and short delays”.
In 2022, the Commission also launched the European Declaration on Digital Rights and Principles. This underlines the commitment to a secure, safe, and sustainable digital transformation that puts people at the centre and reflects the EU’s core values and fundamental rights. In February 2023, the Commission presented its 'connectivity package', including the draft Gigabit Infrastructure Act, a draft recommendation to promote Gb connectivity, and an exploratory consultation on the future of electronic communications infrastructure including the network cost contribution debate. The aim of the package is to provide 1 Gb/s connectivity to all citizens and businesses across the EU by 2030. This is in line with the objectives of the EU Digital Decade policy programme 2030, which also targets 5G coverage for all populated areas by 2030.