Bridging UK and France with Electricity
A new France power interconnector awarded to Prysmian by IFA2 will allow up to 1,000 MW to be transmitted between the countries
A new France power interconnector awarded to Prysmian by IFA2 will allow up to 1,000 MW to be transmitted between the countries
Massimo Battaini, Senior Vice President Energy Projects at Prysmian, is “delighted” to have been selected by two of the Group most important customers, in a deal that “highlights our worldwide market and technological leadership in submarine cable transmission systems”.
Inaddition to the HVDC cable link, the contract includes a High Voltage Alternating Current (HVAC) link that will connect the converter station to a local substation in Chilling, UK, including 2 km land sections at each end with a 5 km subsea section in the between.
The subsea cables will be manufactured in the Prysmian production facility in Pikkala, Finland, whilst the land cables will be manufactured at in Gron, France. The installation of the land sections will also involve resources and facilities from Prysmian France and Prysmian UK, that are headquartered in the nearby area. The Prysmian cable laying vessels Cable Enterprise and Ulisse will work at the installation.
Partnering to IFA2 project, Prysmian will thus provide its contribution to enhance the security, affordability and sustainability of energy supplies in France and Great Britain.
The 1,000 MW high voltage direct current (HVDC) electrical interconnector, will indeed reduce the cost of electricity for homes and businesses in Great Britain, while increasing security of electricity supplies for both countries and providing opportunities for shared use of renewable energy.
The project partners, National Grid and Réseau de Transport d'Electricité (RTE), are planning to complete the construction of IFA2 and start operations in 2020.
OIL & GAS
FAST TRACK PROJECT
FT-ETNO SUMMIT 2017
TELECOMUNICAZIONI
GRADUATE PROGRAM
PEOPLE