1025x580iStock-615803510 - Wheatstone LNG - Copy.jpg

Wheatstone LNG

The Wheatstone LNG facility on the coast of Western Australia is a major new greenfield energy facility. Gas from the Wheatstone, Iago, Julimar & Brunello fields is mixed and fed into the Wheatstone platform, one of the largest integrated production facilities in the world and then transported to shore in a 225 km pipeline




Partners of Choice

Chevron’s Wheatstone LNG facility includes two LNG production trains that will initially produce 8.9 million tonnes of LNG per year, a 200 terajoule domestic gas plant with associated gas processing facilities, LNG condensate and storage facilities and a port for material offloading and LNG export jetty.

Prysmian was chosen to supply all the onshore power, control, instrumentation and telecom cables and is providing a range of services to make sure the project stays on schedule.

Global Reach

Plants in Australia, the Netherlands, USA, Italy and Spain have all made important contributions manufacturing 132 kV High Voltage cables and accessories, Medium and Low Voltage and Control, Instrumentation and Fibre Optic cables that deliver superior performance in the harsh environment of Western Australia where they need to resist very high levels of UV radiation and attack from termites.

This project demonstrates the advantage of working with Prysmian. Our Australian manufacturing and services team applied our experience of supplying multiple LNG projects in Australia over the past ten years. They coordinated the design and delivery of cables from seven Prysmian factories in five different countries and called on the specialist design and manufacturing capacity in Europe for instrumentation and custom designed cables for VFD and fieldbus. 

Local Expertise

In total six million metres of cable have been supplied on over 4,000 cable drums. To make sure the project received the right material at the right time, Prysmian provided a cable management service, including storage & cutting, from our Kewdale warehouse in Perth, WA. This ensured all Chevron’s project milestones were met while minimising cable waste and carefully managing costs.

Products

Pipelines & LNG

The Prysmian range of cable systems for midstream applications delivers innovative solutions for oil and gas pipeline and LNG liquefaction and regasification applications.

arrow-right arrow-right-strong Discover more