Reference Cases  -  About elevator - Elevator - Markets - Prysmian Group

Prysmian group - logo

Prysmian - Draka - logo

Global

Twitter Facebook Linkedin Youtube

Elevator reference cases

??? Image[1]/Titolo ???

World Trade Center

Draka Elevator was selected to provide custom-designed elevator cables and accessories by two major global OEM elevator companies that are performing the rebuilding of the prestigious World Trade Center complex in New York City. Buildings 1 and 4 are now underway. 

??? Image[1]/Titolo ???

Burj Khalifa

Rising more than 2,700 feet (828 m) above the Indian Ocean, the Burj Khalifa is the world’s tallest structure. It is served by 57 elevators moving at speeds of up to 22 mph (10 m/sec). Operating conditions are, to say the least, demanding.